AXIS#.PL.CMD
Description
AXIS#.PL.CMD reads the position command as it is received in the position loop entry.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read Only |
Units | Rotary: counts, rad, deg, custom units, 16-bit counts. See Position Units for details. |
Range | Depends on units. See Position Range for details. |
Default Value | N/A |
Data Type | Float |
See Also | AXIS#.PL.FB |
Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.PL.CMD |
6062h |
00h |
Signed32 |
Position |
- |
Read only |
Yes |
AXIS2.PL.CMD |
6862h |
00h |
Signed32 |
Position |
- |
Read only |
Yes |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.PL.CMD |
5900 |
170C |
Signed32 |
Read Only |
Position |
AXIS2.PL.CMD |
71436 |
1170 |
Signed32 |
Read Only |
Position |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.PL.CMD |
5900 |
Signed32 |
Read Only |
Position |